Terminology

This table defines the terms that are used in this publication.
Terminology
Acronym
Full Term
Definition
BP
Backplane Power
Power that is generated from module power by the adapter and expansion power, and supplied to the I/O system through the backplane.
CIP™
Common Industrial Protocol
An industrial communication protocol that is used by Logix 5000® based automation systems on EtherNet/IP™, ControlNet®, and DeviceNet® communication networks.
CIP Sync™
Common Industrial Protocol Synchronization
CIP Sync provides the increased control coordination needed for control applications where absolute time synchronization is vital to achieve real-time synchronization between distributed intelligent devices and systems.
CJC
Cold Junction Compensator
A device that is used in thermocouple measurements to help obtain accurate temperature readings at the hot junction.
DAC
Digital to Analog Converter
A device converts digital signals into analog signals, enabling seamless communication between digital devices and analog systems.
DCE
Data Communications Equipment
A device that facilitates data transmission over a network.
DTE
Data Terminal Equipment
A device that serves as a communication endpoint in a network.
HART
Highway Addressable Remote Transducer
A protocol that enables both analog and digital communication over the same wiring, including device diagnostic and status information.
HSC
High-speed Counter
A device that is used to count input signals at a rapid rate. Typically associated with incremental encoders.
LA
Local Actuator - Power
Local Actuator Power supplied through the RTB.
MB
Mounting Base
A device that provides data and power connections from the backplane to the installed module.
MP
Module Power
Power that is supplied to the adapter and expansion power.
MSB
Most Significant Bit
The bit that has the largest value in a multi-bit binary number.
MTO
Motor Torque Off
A motor control function that disables torque generation by removing torque-producing drive output from the motor.
NFC
Near Field Communication
A short-range wireless technology that enables communication between two electronic devices over a distance of 4 cm (1.6 in.) or less.
ODVA
Open DeviceNet Vendor Association
A nonprofit association of vendors that are established for the promotion of CIP networks.
PL
Performance Level
ISO 13849-1 safety rating
RIUP
Removal and Insertion Under Power
A feature that enables the device to be connected and disconnected from the system without having to remove power from the system.
RPI
Requested Packet Interval
Time interval (usually in milliseconds) that users are requesting their data be exchanged at
RTB
Removable Terminal Block
A component that is used for wiring field devices to.
RTD
Resistance Temperature Detector
A type of sensor whose resistances change as its temperature changes.
SA
Sensor Actuator - Power
Sensor Actuator Power (24V DC nominal) for the field devices.
SELV
Safety Extra Low Voltage
An electrical system where the voltage level is considered safe under normal or fault conditions, as defined in the EN and IEC standards.
SIO
Standard Input/Output
Describes the function of a port on an IO-Link master device.
SSI
Serial Synchronous Interface
A serial communication standard for transmitting data between a leader device and a follower device. Typically associated with absolute encoders.
SSV
Sensor Source Voltage
Voltage that is supplied to a sensor.
VCL
Voltage Clamp Low
The low threshold for limiting the voltage level.
XT
Extreme Environment
Modules with XT at the end of their catalog numbers have design considerations and conformal coating that add a degree of protection for harsh, corrosive gas environments.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal