I/O Modules Status Indicators
PointMax I/O modules include status indicators such as SA power, LA power, module
status, and I/O channel status to indicate module operating conditions and behavior.
Not all I/O modules include an SA power status indicator. Some modules, such as AC
I/O modules, include an LA power status indicator. For more information about these
indicators, see PointMax I/O System Specifications Technical Data, publication 5034-TD001.
For detailed, module-specific status indicator information, see the module user
manual listed in the Additional Resources.
SA Power Status Indicator
Indicator State | Description |
|---|---|
Steady red | One of the following:
|
Steady green | The SA power is in the valid range. |
LA Power Status Indicator
Indicator State | Description |
|---|---|
Steady red | There is no LA power to the module or LA power is not in the
valid range. |
Steady green | The LA power is in the valid range. |
Module Status Indicators
Indicator State | Description |
|---|---|
Off | The module is not powered. |
Steady red | The module experienced a nonrecoverable fault. |
Flashing red and green | The device is in a self-test mode. |
Flashing red | One of the following conditions exists:
|
Flashing green | The module has no I/O connections. |
Steady green | The module is operational and all I/O connections are active. |
I/O Channel Status Indicators
Indicator State | Description |
|---|---|
Off | One of the following:
|
Steady yellow | One of the following:
|
Flashing red | A fault condition is detected. Examples include field power
loss, a short circuit condition, an open wire, or an
overrange condition. |
Indicator State | Description |
|---|---|
Off | One of the following:
|
Steady yellow | The point is operating normally. |
Flashing red | The module experienced one or more recoverable faults. |
Steady red | One of the following:
|
Provide Feedback