System Planning
Follow these rules when planning your system configuration:
- The adapter is the leftmost component in the rack when in horizontal mounting.
- Local PointMax I/O modules are installed to the right of the adapter.
- The 5034-AENTR and 5034-AENTRXT adapters support a maximum of 16 I/O modules. You can expand the rack to 32 I/O modules with an expansion power (5034-EXP or 5034-EXPXT) between the two sets of 16 I/O modules.
- Before powerup, verify that the end cap is installed on the last mounting base (MB) in the PointMax I/O system.
- For vibration or shock environments, verify that DIN rail end anchors are installed at both ends of the system.
Provide Feedback