Remove and Replace the Adapter Network Address Door
To reduce the risk of damage to the door hinges follow these step to safely remove the
adapter network address door:
- Lift the network address door using the tab.
- Pivot the door up until the door hinges disengage from the adapter hinges.
Provide Feedback