Error - Failed to add the open project to source control

Failure to add the open project to source control.
A possible reason may be compatibility problems between the version of FactoryTalk AssetCentre for source control and the Logix Designer application.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal