From a P-controller to another P-controller, or to another platform, or from another platform

When you switch between P-controllers, or controllers that do and do not support Process instructions, these conditions apply:
From a P-controller to a P-controller
When you change from a controller that supports Process instructions to another controller that supports Process instructions, functionality does not change for the Process instruction.
From a P-controller to a non-P-controller
When you change from a controller that supports Process instructions to a controller that does not support Process instructions:
  • Process instruction data type tags and Process instructions within routines do not change. The instructions remain in the program, but they are invalidated. You cannot download projects that contain Process instructions. Routines that contain Process instructions fail verification.
  • The
    Logix Designer
    application deletes process instruction template alarm definitions.
  • The tasking model and instruction usage options are no longer available.
From a non-P-controller to a P-controller
When you change from a controller that does not support Process instructions to a controller that does support Process instructions, the
Logix Designer
application creates template alarm definitions for the Process instructions. The tasking model and instruction usage options are available for use.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal