New Project dialog box
Use the
New Project
dialog box to configure project options for a new Logix Designer
™ project.Most controllers display the standard project configuration options. The CompactLogix 5370,
CompactLogix 5370 L1, ControlLogix 5580, and ControlLogix 5590 controllers display unique
project configuration options.
To open the New Project dialog box:
- From the Studio 5000 launcher, selectNew Project.
- In theProject Typescolumn, selectLogix.
- Locate the controller for this project by expanding each controller category in the list or by typing a search term in the search bar.
- Select a controller from the list.
- In theNamebox, type a name for the project file. The name is limited to 40 characters and must meet the IEC-61131 Name standard.
- (optional) In theLocationbox, type or browse to a location to store the project file.
- SelectNext.
Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.
Provide Feedback