Module Properties - RSNetWorx for ControlNet

Use this tab to:
  • launch RSNetWorx for ControlNet to view and/or edit the respective network
  • associate a ControlNet project file with the respective module
  • schedule a ControlNet network
Parameters
ControlNet File (.xc)
Displays the name of the ControlNet file you want to associate with the module. By default, this field is blank.
Browse
Click this button to search for the file you want to associate with the module.
Found In
Displays the location where the network file was found. If no file was found, this field does not appear on the dialog.
LaunchRSNetWorxButton Launch RSNetWorx for ControlNet button
Click this button to launch RSNetWorx for ControlNet, from which you can:
  • save the current network data into the ControlNet project file (*.xc).
  • view and/or edit the network
  • schedule a ControlNet network
You must also apply any pending edits before you can launch RSNetWorx.
For ControlNet networks, this button is not enabled until:
  • you have specified a ControlNet project file
  • you have specified a slot number and a node number for the ControlNet scanner
Status
Displays the status the controller has about the module:
This status:
Indicates:
Standby
a transient state that occurs when shutting down
Faulted
the controller is unable to communicate with the module
When the status is Faulted, the Connection tab displays the fault.
Validating
a transient state that occurs before connecting to the module
Connecting
a state that occurs while the connection(s) are being established to the module
Running
the module is communicating and everything is working as expected
Shutting Down
the connections are closing
Inhibited
the connection to the module is inhibited
Waiting
a connection to this module has not yet been made due to one of the following:
  • its parent has not yet made a connection to it
  • its parent is inhibited
  • its parent is faulted
Offline
you are not online
OK
Click this button to accept your edits on any tab and close the dialog.
Cancel
Click this button to cancel your edits on any tab and close the dialog.
Apply
Click this button to apply your edits on any tab and continue editing.
Help
Click this button for help on this tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal