Create an equipment phase

Use this procedure to create an equipment phase.
To create an equipment phase:
  1. In
    Name
    , enter a name for the equipment phase.
  2. In
    Description
    , enter a description of the phase (optional).
  3. From the
    Schedule in
    menu, choose the task in which to schedule the equipment phase.
    The list will contain only those tasks in which the equipment phase can be scheduled.
    TIP:
    If creating the equipment phase by right-clicking a task in the
    Controller Organizer
    , the chosen task is already selected in this field.
  4. Select
    Inhibit Equipment Phase
    to prevent the controller from executing this equipment phase.
    If selected, the equipment phase is still prescanned. If the equipment phase is then enabled when the controller is already in Run mode, the equipment phase is not prescanned again.
  5. (optional) If necessary, note the
    parent
    program displayed for the equipment phase.
  6. Select
    Synchronize Redundancy Data after Execution
    to synchronize data at the end of the phase execution.
  7. Select
    OK
    to create the equipment phase.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal