Customize the Language Element Toolbar

To customize the Language Element toolbar:
  1. From the
    Language
    menu, choose the language of the toolbar you want to modify.
  2. Add and remove buttons to configure your toolbar.
    Select the
    arrow
    buttons to add and remove toolbar buttons.
  3. Select
    OK
    to accept your toolbar configuration.
  4. Select
    Close
    to close the
    Customize Toolbar - Language Element
    dialog box.
To access the Customize Toolbar - Language Element dialog box
To access the
Customize Toolbar- Language Element
dialog box, from the
View
menu, choose
Toolbars
.The
Toolbars
dialog box opens. Select the
Language Element toolbar
from the list. Select
Customize
.The
Customize Toolbar - Language Element
dialog box opens.
TIP: If FactoryTalk Security is enabled, this dialog may be disabled, depending on the levels of access that have been defined. For details about FactoryTalk Security see FactoryTalk Help:
Start > Programs > Rockwell Software> FactoryTalk Help
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal