Position Loop page
Use the settings on the
Position Loop
page in the Axis Properties
dialog box to configure the position loop of the axis.
TIP:
To open the Position Loop page:
- In theController Organizer, expand theMotion Groupsfolder, then right-click the axis and selectProperties.
- From theAxis Propertiesdialog box, inCategories, selectPosition Loop.
Parameter | Description |
|---|---|
Bandwidth | Enter a bandwidth value in Hertz. |
Integrator Bandwidth | Enter an integrator bandwidth value in Hertz. |
Integrator Hold | Enable or disable for the integrator during commanded motion. |
Velocity Feedforward | Enter a percentage for the Velocity Feedforward. |
Error Tolerance Limit | Enter a value for the position error tolerance in Position Units. |
Lock Tolerance | Enter a value for the position lock tolerance in Position Units. |
Parameters | Opens the Motion Axis Parameters page to modify existing or additional parameters.
TIP:
The
Parameter List page may contain more
attributes than the associated page. In some cases, attributes that display on the
Parameter List page do not display on the associated page. |
Provide Feedback