General page
The
General
page establishes key associations and operations for the axis. Axis attributes are required, optional, or conditional based on the selected control mode. Use the General
page to:- Associate axes and drivesIMPORTANT: Be sure to associate the drive as the first step in configuring the axis. The drive determines which attributes are supported.
- Configure the associated axis and control mode
- Create and associate a new motion group
- Manually change tuning and issue motion direct commands.
TIP:
To open the General page:
- In theController Organizer, expand theMotion Groupsfolder, and double-click an axis.
- From theAxis Propertiesdialog box, inCategories, clickGeneral.
The parameters displayed in the
General
page depend on the type of Axis Configuration, drive selected, and controller capabilities.Parameter | Description |
Axis Reset | Re-initializes the axis to its default state and restores the last applied Module, Axis Number, and Motor Catalog Number. Automatically updates all dependent attributes. This operation cannot be undone. |
Axis Configuration | Selects an axis type from the list. The available options are:
|
Feedback Configuration | Determines how the available feedback channels of the drive associate with this axis. The Feedback Configuration options vary by profile and axis type. |
Application Type | Determines the type of motion control application. Defines the servo loop configuration automatically. These combinations determine how to make calculations and reduces Autotuning and Manual tuning. The available values include:
TIP:
Changing the
Application Type value
affects other attributes (Velocity Integrator Hold , Position
Integrator Hold , Gain Tuning Configuration Bits ).Application Type is unavailable when the axis is Servo On . |
Converter Configuration | Determines the general control behavior of the regenerative or low harmonic AD/DC converter axis. The available values include:
|
Loop Response | Selects how tightly or hot the system tunes. The available values include:
The default value is the current value of the attribute.
TIP:
Changing the
Loop Response value
affects the Damping Factor attribute.Loop Response is unavailable in online mode and when the axis is Servo On . |
Vertical Load Control | Tailors motor control behavior for vertical load applications. When Enabled , the drive attempts, whenever possible, to avoid applying Category 0 stop actions in response to Major Fault conditions. The drive may tailor other aspects of its behavior to best handle vertical loads.The available values include:
|
Converter Startup Method | Specifies how the regenerative axis transitions from the Stopped state to the Starting state. The available values include:
This parameter is unavailable in online mode and when the axis is Servo On . |
Reactive Power Control | Enables or disables the reactive power control function for the regenerative converter. When Enabled , the regenerative converter works solely as a reactive power compensation device by injecting reactive power to the grid. The converter does not transfer active power to associated drives on the DC Bus. Instead all of the converter's rating capacity is dedicated to reactive power correction to the grid.The available values include:
This parameter is unavailable in online mode and when the axis is Servo On . |
Motion Group | Associates a motion group to the axis. Select <none> to not associate a motion group with the axis. The motion_group value is selected by default. Click to open the Axis Properties dialog box. is unavailable when there is no axis associated with the node and when there are pending edits. |
New Group | Opens the New Program Parameter or Tag dialog box to create a new motion group.New Group is unavailable in online mode, when the maximum number of groups has been exceeded, and when the axis is not associated with a drive. |
Update Period | View the update period for the axis. Shows the Base Update period by default. Or, if applicable, shows the multiplex update rate. Click to open the Axis Schedule dialog box to schedule the base update period and alternate 1 and alternate 2 periods, and assign axes to the rates. |
Module | Associates the motion module with this axis. Changing the module changes the profile of the module and the options the module supports. |
Modular Type | Identifies the motion module type (read-only). |
Power Structure | Identifies the power structure used with the module (read-only). |
Axis Number | Selects the axis number of the motion module. The available options are Axis 1, 2, 3, or 4. Axis numbers that are already assigned do not appear in the list. |
Application Catalog Number | The catalog number of the robot that this axis belongs to.
TIP:
When an axis is associated to a robot, it
might be managed, meaning some axis parameters are not configurable depending on
the robot type. Refer to the specific robot documentation for a list of
configurable parameters.
|
Application Version | The current version of characterized data for the application. |
Instance | The unique identifier assigned by Application Code Manager to all objects in the system that comprise one application. For example, for a robot, the application is the coordinate system and all joint axes. All of these objects receive the same instance number to indicate that they are part of a specific application. |
Axis Test Mode Enable | Activates or deactivates Axis Test Mode. When Axis Test Mode Enable is enabled, the test mode status appears at the bottom of both the General page and the Controller Organizer .
TIP:
Axis Test Mode is available if it is supported by the selected
controller.
|
Axis Test Mode Configuration | Determines the configuration for the Axis Test Mode. |
Provide Feedback
to open the