System features

Logix Designer application version v38.01 has these new and enhanced features.
New features
Enhanced features
  • Check box enables and disables alerts when read-only tag members are overwritten
    In this version of the Logix Designer application, you can select the
    Enable Programming Practices Guardrail for Output Tag Member Overwrites
    check box to view alerts in the Errors tab of the Output window. When a read-only tag member is overwritten, this message appears in the
    Errors
    tab of the
    Output
    window: Tag member overwrites may cause unexpected errors/behaviors. When you clear the check box, the alerts do not appear. This option is selected by default.
  • New Timer_T data type
    This version of the Logix Designer application includes the TIMER_T data type. The TIMER_T data type:
    • Further integrates the DateTime feature into the Logix Designer instruction set. You can set the Timer operand as TIMER or TIMER_T in the Timer On Delay (TON), Timer Off Delay (TOF), and Retentive Timer On (RTO) instructions. The TIMER_T data type has Accumulated (ACC) and Preset (PRE) members whose data type is TIME.
    • Clarifies elapsed time by displaying values in units of time: days (d), hours (h), minutes (m), seconds (s), milliseconds (ms), and microseconds (us). You no longer need to derive ACC or PRE values from a DINT that represents milliseconds.
  • FGEN instruction supported in safety applications
    In this version of the Logix Designer application, you can use the Function Generator (FGEN) instruction in safety applications.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal