Use the Module Browser
The Module Browser lists all the:
- InOut parameters in the program scope with the MODULE data type. This list appears when the parameter expects a module reference parameter. These appear under theParameterslabel. From this browser, you can choose the parameter you wish to use, simply by selecting it from the Parameter list.
- Modules in the current controller for which you have provided names. From this browser, select the module from the Module list. The module path is placed in thePathfield in theMessage Configurationdialog box, and its name is displayed underneath it.
The browser only works if the selected module has a name.
To specify a message path to a module that is unnamed:
- Select the parent module (which must have a name)
- Add the remainder of the path in numeric form
For example, "MyCNBAdapter,1,3" would indicate a path leading to a remote CNB module named MyCNBAdapter and then continuing across the backplane to the unnamed module in slot 3.
![]() | Select Show Tree View to show the module list as a tree, such as the Controller Organizer , or a flat list. |
Provide Feedback