Program Properties Dialog Box - Monitor Tab Overview

Monitor program scan times from this
Monitor
tab of the
Program Properties
dialog box.
The following table provides descriptions of the parameters available.
Parameter
Description
Scan Time - Max
Displays the largest scan time since the last Reset.
Scan Time - Last
The the time used for this task from the previous scan.
Reset Max
Click this button to reset the scan time values.
OK
Click this button to apply your edits and close the
Program Properties
dialog box.
Cancel
Click this button to cancel your edits and close the
Program Properties
dialog box.
Apply
Click this button to apply your edits and continue editing in the
Program Properties
dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal