SLC 500: timer, counter, and control files
This addressing syntax applies to Fixed I/O SLC, SLC 5/01, SLC 5/02, and SLC 5/03 OS300.
Fnnn:eee.MNE/bb
F | (file type) | |
T | Timer | |
C | Counter | |
R | Control | |
nnn | (optional file number) | |
Timer | 4, 9-255 decimal | |
Counter | 5, 9-255 decimal | |
Control | 6, 9-255 decimal | |
Timer, counter and control file types use the default file number if the file number is absent. The default numbers are 4 (timer), 5 (counter), and 6 (control). | ||
eee | (element number) | 0-255 decimal |
MNE | (member mnemonic) | |
bb | (optional bit number) | 0-15 decimal |
Applies to analog members only. | ||
Example
R167:123.EN |
Provide Feedback