Activate FactoryTalk Optix Runtime on online devices
Activate a Runtime entitlement through License Manager on a Runtime online device.
- Open License Manager using either the Windows Start menu or the icon on your desktop.
- SelectOnlineto activate a new entitlement on the Runtime device.
- SelectActivate an entitlement for this deviceandNext.Your entitlement key is a 25-character key created by FactoryTalk Optix used to allocate an entitlement to an organization.
- Access the FactoryTalk Optix landing page.
- Authenticate as required.
- SelectEntitlementsto view and copy the entitlement key.
- Enter the Entitlement Key and selectActivate.
- When the entitlement activates successfully, selectOK.
- SelectEntitlementsagain, and thenOrganization entitlementsto display the allocated entitlement.
NOTE:
When you deploy FactoryTalk Optix Applications to the Runtime device, all required Runtime files automatically deploy with the application.
Provide Feedback