OptixEdge Standard
OptixEdge
StandardOptixEdge
Standard is an industrial edge gateway that is equipped
with an NXP i.MX 8M Plus processor.OptixEdge
Standard can connect to the cloud via
FactoryTalk® Optix™
, provide remote assistance via FactoryTalk® Remote
Access™ with embedded digital I/O, and host Docker® containers. OptixEdge
contains a
FactoryTalk® Optix™
Runtime
base package XS or base package S entitlement, depending on the model. An upgrade from
base package XS to base package S is also available. For more information, see .
OptixEdge
Standard User Manual,
publication 2800E-UM001OptixEdge
StandardSee Table 1 for software and token information.
Provide Feedback