Terminology

This table defines terms that are used in this publication.
Terminology
Term
Definition
Activate a
FactoryTalk® Hub™
Entitlement
The process of either assigning an entitlement to a runtime target device or a myRockwellAutomation User. The process is the same to upsize an existing entitlement.
Activation is typically performed by The myRockwellAutomation User who is a member of the
FactoryTalk® Hub™
organization to which the entitlement is allocated.
Advisor
A cloud-based platform for product selection, configuration, bill of materials management, and more. Available through
FactoryTalk® Hub™
.
Allocate a
FactoryTalk® Hub™
Entitlement
After purchase of a
FactoryTalk® Optix™
or
FactoryTalk® Remote Access™
entitlement, you must allocate the entitlement to the appropriate FactoryTalk Hub organization before it can be used.
The myRockwellAutomation User who placed the order on the Rockwell Automation Software Commerce Portal typically allocates the entitlement.
Application Code Libraries/Trusted Content
Preconfigured content that is developed, managed, and made available from Rockwell Automation at no additional cost to help expedite project creation and project maintenance.
Container
A containerized software deployment. A container is a way to package an application and its requirements into one unit, making the application portable and easier to manage. See FactoryTalk Optix Studio Applications as Container Solution.
Devices with Optix embedded
Specific Runtime Target Devices that come from
Rockwell Automation®
preloaded with the software and entitlements for
FactoryTalk® Optix™
Runtime Tools and
FactoryTalk® Remote Access™
Runtime. Access to the operating system in these devices is restricted (closed system).
See Table 1.
Entitlement
The license that is required to run
FactoryTalk® Hub™
software, such as
FactoryTalk® Optix™
and
FactoryTalk® Remote Access™
.
FactoryTalk® Design Studio™
A cloud-based design platform that enables teams to work on projects involving multiple controllers. Available through
FactoryTalk® Hub™
.
FactoryTalk® Hub™
A cloud-based platform, which serves as a central access point for Software-as-a-Service (SaaS) offerings.
FactoryTalk® Hub™
is accessible via FactoryTalk Hub and requires a MyRockwellAutomation account to sign in.
Some
FactoryTalk® Hub™
products require the purchase of a license to operate.
FactoryTalk® Hub™
Organization
An organization acts as a grouping for myRockwellAutomation Users, licenses, and access rights within
FactoryTalk® Hub™
, which enables collaboration and resource sharing.
It is free to create or join an organization and required to use
FactoryTalk® Hub™
.
FactoryTalk® Optix™
A cloud-enabled Human Machine Interface and IIoT platform. Available through
FactoryTalk® Hub™
.
FactoryTalk® Optix™
Application
The project that is developed in
FactoryTalk® Optix Studio™
and compiled to run.
FactoryTalk® Optix™
Entitlement
Available in several package sizes consisting of a quantity of feature tokens. The entitlement can be upsized to a larger package size at any time.
Also available as perpetual entitlement with maintenance or a subscription. A perpetual entitlement is included with some runtime target devices with an optional one-step upsize of the perpetual entitlement available.
See Table 1.
FactoryTalk® Optix™
Runtime Tools
FactoryTalk® Optix™
runtime software that is used to run a
FactoryTalk® Optix™
Application.
FactoryTalk® Optix Studio™
FactoryTalk® Optix™
design-time software
FactoryTalk® Optix Studio™
Entitlements
Available in two options: Standard (free) or Pro (paid subscription).
FactoryTalk® Remote Access™
A cloud-based solution that enables secure remote connectivity to industrial automation equipment. Available through
FactoryTalk® Hub™
.
FactoryTalk® Remote Access™
Manager
A web-based interface for managing remote connections to industrial automation systems with a
FactoryTalk® Remote Access™
Runtime.
FactoryTalk® Remote Access™
Manager Entitlement
Available as a subscription based on the number of concurrent users. The number of concurrent users is how many users can connect to remote devices simultaneously, not the total number of users that can use the software.
FactoryTalk® Remote Access™
Runtime
Software that allows you to establish secure, remote connections to industrial equipment from the
FactoryTalk® Remote Access™
Manager.
FactoryTalk® Remote Access™
Runtime Entitlement
Available as a perpetual entitlement or a subscription. In either Basic or Pro levels. A perpetual entitlement is included with some hardware. Upsizing from Basic to Pro is available.
See Table 1.
Feature Tokens
The number of feature tokens determines the size of a
FactoryTalk® Optix™
Runtime Entitlement. See Table 2.
myRockwellAutomation
A centralized user access platform from
Rockwell Automation®
that provides a personalized experience by bringing together a wide range of digital tools and resources, including product information, software subscriptions, support documentation, Knowledgebase articles, and more.
Access and create a free account at www.myRockwellAutomation.com.
myRockwellAutomation User
The email address that is registered with myRockwellAutomation.
Offline
The runtime target computer is not on a network that can be routed to
FactoryTalk® Hub™
.
Online
The runtime target computer is on a network that can be routed to
FactoryTalk® Hub™
.
Examples of online scenarios:
  • Your local computer is remote from the runtime target computer and they both have access to networks that can be routed to
    FactoryTalk® Hub™
    .
  • Your local computer is remote from the runtime target computer and they both have access to the internet.
Purchase
  • Purchase Rockwell Automation software through the Rockwell Automation Software Commerce Portal or from your local Allen-Bradley distributor.
  • Purchase Rockwell Automation hardware through your local Allen-Bradley distributor.
Rockwell Automation Software Commerce Portal
Also known as the Subscription Portal, compliments Rockwell Automation’s network of authorized distributors by serving as a centralized ecommerce platform for software purchases, subscription management, and more.
Access to the Rockwell Automation Software Commerce Portal requires a MyRockwellAutomation account to sign in.
  • Subscription licensing – Provides access to the software for an annual fee. Subscription license includes ongoing support and software updates.
  • Perpetual with maintenance licensing - Grants the right to use the software indefinitely after a one-time cost with the first year of maintenance included. The maintenance component can be a recurring fee when ongoing support and software updates are needed.
Runtime Target Computer
Specific Runtime Target Device that is either an
ASEM™
6300 industrial computer or any PC or virtual machine that runs
Windows®
or Linux operating system. Access to the operating system in these devices is not restricted (open system).
Runtime Target Device
The compute device that you use to run the
FactoryTalk® Optix™
Application.
Types of Runtime Target Devices include:
  • Runtime Target Computers
  • Devices with Optix embedded
See Table 1.
Software-as-a-Service (SaaS)
A software distribution model that allows access to software through a web browser or app instead of installing and managing software on a PC or device.
Virtual Machine
Virtual version of a physical computer, which allows multiple operating systems and applications to run on one physical computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal