Create an interface for filtering numeric data

Create a text box that enables you to filter motor properties based on queries entered.
  1. Create the query filter text box:
    1. Right-click
      MainWindow (type)
      and select
      New
      Base controls
      Text box
      .
    2. Hover-over the text box, select
      Edit
      , and enter
      NumericFilterTextBox
      .
    3. In
      Properties
      , create a dynamic link between
      Text
      and
      ProjectName
      UI
      MotorNumericGrid
      Query
      .
      For more information about dynamic links, see Create dynamic links.
    4. Set
      Placeholder text
      to
      SELECT * FROM Model WHERE
      {Conditions}
      .
  2. Create the query filter label:
    1. Right-click
      MainWindow (type)
      and select
      New
      Base controls
      Label
      .
    2. Hover-over the label, select
      Edit
      , and enter
      NumericFilterLabel
      .
    3. In
      Properties
      , set
      Text
      to
      Filter motors:
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.