Create a list box

Create a list box that enables you to switch between Motor and Kiln objects.
  1. In
    Project view
    , right-click
    MainWindow (type)
    and select
    New
    Data controls
    List box
    .
  2. In
    Properties
    , create a dynamic link between
    Model
    and
    ProjectName
    Model
    .
    For more information about dynamic links, see Create dynamic links.
  3. Expand
    Model
    and create a dynamic link between
    ItemKind
    and
    Types
    ObjectTypes
    Object
    .
    For more information about dynamic links, see Create dynamic links.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.