Create an alarm trigger

Create a switch that triggers the ConveyorChassisMalfunction alarm.
  1. Create a switch that triggers the alarm:
    1. In
      Project view
      pane, right-click
      MainWindow (type)
      and select
      New
      Base controls
      Switch
      .
    2. Hover-over the switch, select
      Edit
      , and enter
      TriggerConveyorChassisMalfunctionAlarm
      .
    3. In
      Properties
      , create a dynamic link between
      Active
      and
      ProjectName
      Model
      ConveyorChassisMalfunctionAlarmVariable
      .
      For more information about dynamic links, see Create dynamic links.
  2. Create a trigger label:
    1. In
      Project view
      , right-click
      MainWindow (type)
      and select
      New
      Base controls
      Label
      .
    2. Hover-over the label, select
      Edit
      , and enter
      TriggerAlarmLabel
      .
    3. In
      Properties
      , set
      Text
      to
      Trigger the conveyor chassis malfunction alarm:
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.