Create a list of motors

Create a list box populated with motor objects.
  1. In
    Project view
    , right-click
    MainWindow (type)
    and select
    New
    Data controls
    List box
    .
  2. Hover-over the list box, select
    Edit
    , and enter
    MotorListBox
    .
  3. In
    Properties
    , create a dynamic link between
    Model
    and
    ProjectName
    Model
    MotorObjects
    .
    For more information about dynamic links, see Create dynamic links.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.