Create a severity color converter

Create a converter that translates alarms severity into colors.
  1. Create the converter:
    1. In
      Project view
      , right-click
      Converters
      and select
      New
      Key-value converter
      .
    2. Hover-over the converter, select
      Edit
      , and enter
      SeverityColorConverter
      .
  2. Configure the converter:
    1. Double-click
      SeverityColorConverter
      .
    2. In the central pane, next to
      Values
      , select
      String
      and select
      Color
      .
      TIP: If you do not see the required option, select the
      Show all
      checkbox.
    3. Add another row by selecting
      Add
      .
    4. Enter the following values:
      Keys (UInt32)
      Values (Color)
      1
      #ff0000
      0
      #0664c2
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.