Channel values too close
One or more of these scenarios may be true:
- Low Engineering and High Engineering values are equal.
- High Signal value is less than Low Signal value.
- Low Signal and High Signal values are equal.
Check the configuration, make the required modifications, and apply the changes.
Provide Feedback