Outputs view parameters
The
Outputs
view includes these parameters:
Parameter | Description |
|---|---|
Output | Displays the output number to which this configuration
applies. |
Mode | Displays the mode for the output. |
Output State in Program Mode | Determines the behavior of each output when the controller
transitions to Program Mode or Inhibit mode. While in Program
Mode or Inhibit mode, outputs from the controller are ignored
and the output behaves as follows:
|
Output State in Communication Fault Mode | Determines what happens to the output of each point after a
communication fault occurs and the module enters Communication
Fault Mode.
|
Diagnostics | Opens the Diagnostics dialog, which contains diagnostic
information. |
Provide Feedback