Disabling HTTP and SNMP servers interrupts access to device web pages and SNMP clients
Selecting
Set
in the Servers
view writes changes to the device. If you disable
the SNMP and HTTP servers and select Set
, it interrupts access to the SNMP clients and
the device web pages.Ensure an interruption now is acceptable, and select
Yes
to apply the changes. Select
No
to cancel the operation.Provide Feedback