Configure the port settings
Use the
Port Configuration
view to configure the port settings for
non-controller devices.Prerequisites
- You must be online and communicating with the device.
- Ensure a connection interruption at this time is acceptable.IMPORTANT:Configuring the port settings requires data to be written to the device, which interrupts the connection to the device and to any other device that is connected through it. Connections from other controllers may be interrupted as well. You must not interrupt the connection on a device that is currently being used for control.
To configure the port settings
- On the tab for the device, selectPort Configuration.
- In thePort Configurationview, configure the settings as needed.
- SelectSetto write the changes to the device.
Provide Feedback