Network view parameters (tap devices)
The
Network
parameters are configurable and the values appear only when online and
there is no communication error in the device profile. The parameters for tap devices include
these parameters.Parameter | Description |
|---|---|
Network mode | Displays the network mode. |
Network topology | Displays the current network topology as either:
|
Network status | Displays the current network status as:
|
Enable supervisor mode | Indicates that the device is configured as a supervisor on the network. If cleared,
the Supervisor Mode is disabled, and the device is not a supervisor on the
network. |
Advanced | Opens Advanced Network Configuration to configure advanced network
properties. |
Supervisor status | Displays the status of the supervisor. Only available when Supervisor Mode
is enabled. Available values:
|
Active ring supervisor | Displays the IP Address or MAC Address of the Active Ring Supervisor. Only available when the device is in Ring network. |
Active supervisor precedence | Displays the precedence currently assigned to the active ring supervisor. Only available when the device is in a Ring network. |
Ring faults detected | Displays the number of ring faults detected on the network since the last power
cycle or counter reset. Only available when the device is a ring supervisor. |
Last active node on Port 1 | Displays the IP address or MAC ID of the last node the active ring supervisor can
communicate with on Port 1 when a ring fault occurred. Only available when the device is a ring supervisor. |
Last active node on Port 2 | Displays the IP address or MAC ID of the last node the active ring supervisor can
communicate with on Port 2 when a ring fault has occurred. Only available when the device is a ring supervisor. |
Status | Displays the current condition of the ring fault as:
Only available when the device is a ring supervisor. |
Reset Counter | Used to reset the device's ring fault count to zero. Only available when the device is a ring supervisor. |
Verify Fault Location | Causes the device to verify the last node fault location on port 1 and port 2 and
update the Last Active Node parameters.The Last Active Node parameters show information from the last fault until
you verify the fault location.Only available when the device is a ring supervisor. |
Clear Fault | Causes the device to clear the Rapid Faults/Restore Cycles fault. Only available when the device is a ring supervisor and the ring fault condition is
Rapid Fault/Restore Cycles . |
Port Buffer Utilization | Displays the percentage of the buffer that is being used for port 1 and port 2. |
Device Port | Displays the percentage of the device port that is being used. |
Refresh | Retrieves and displays the latest information from the device. |
Provide Feedback