Configure the Internet Protocol settings
Use the
Internet Protocol
view to configure the Internet Protocol (IP)
settings for non-controller devices. The Internet Protocol
view is only
available for devices with an embedded EtherNet port.
TIP:
The settings, are read-only when the device is a controller. In addition, the settings
appear shaded and have no value when the device is:
- offline.
- online and a communication error occurs.
- configured using the switches on the device (for those devices that support setting the IP address by switches)
Prerequisites
- You must be online and communicating with the device.
- Ensure a connection interruption at this time is acceptable.IMPORTANT:Configuring the IP settings requires data to be written to the device, which interrupts the connection to the device and to any other device that is connected through it. Connections from other controllers may be interrupted as well. You must not interrupt the connection on a device that is currently being used for control.
To configure the IP settings
- On the tab for the device, selectInternet Protocol.
- In theInternet Protocolview, forInternet Protocol (IP) Settings, selectManually configure IP settings.TIP:To obtain IP settings automatically from a server on the network using either the BOOTP or DHCP protocol, selectObtain IP settings automatically using BOOTPorObtain IP settings automatically using DHCP.
- ForIP Settings Configuration, specify these parameters:
- Physical device IP AddressEnter a unique address used by the IP protocol to route information to and from the device.TIP:If a message appears indicating that the IP address in physical device does not match the one in device properties, selectUse Properties IP Addressto populatePhysical device IP addresswith the data from theOverviewview.
- Enter the extension of the IP address scheme that lets a site use a single net ID for multiple physical networks.
- Enter the address used to connect individual physical networks into a system of networks.
- (optional) Specify the remaining parameters forIP Settings Configuration:
- SelectSetto write the changes to the device.
Provide Feedback