Redundancy view parameters
The
Redundancy
view shows the redundancy status and allows you to qualify or
disqualify the secondary adapter, and switch to the secondary adapter.Parameter | Description |
|---|---|
Primary Adapter Physical Slot | Displays the primary adapter's physical slot.
|
Redundancy Status | Displays the primary or the secondary adapter's redundancy status.
|
Qualify Secondary | Qualifies the secondary adapter. |
Qualification in Progress | Displays the qualification status.
|
Disqualify Secondary | Disqualifies the secondary adapter. |
Switch to Secondary | Switches to the secondary adapter. Tip: Switch to Secondary is disabled while offline or Secondary Compatibility does
not match Primary. |
Provide Feedback