Obtain an authorized Full License

After the Demo License expires, obtain a Full License to continue using the
AADvance-Trusted SIS Workstation software
for AADvance applications.
To obtain a Full License
  1. To start
    AADvance-Trusted SIS Workstation software
    with the
    Windows
    administrator privileges required to manage licenses, right-click the
    SIS Workstation
    Windows
    desktop shortcut and then select
    Run as administrator
    .
  2. From the
    Help
    menu, select
    Licensing AADvance
    .
    The licensing information displays along with three User Codes.
  3. Send an email that contains the required license type and all three
    User Codes
    to the support team:
    keymaster@ra.rockwell.com
  4. The support team emails you back
    Registration Keys
    1 and 2.
  5. From the
    Help
    menu, select
    Licensing AADvance
    .
  6. Enter the registration keys in their respective fields and select
    Validate
    .
    TIP: Ensure the User Codes that appear in the
    AADvance-Trusted SIS Workstation software
    match the ones received in the email. If they differ, use the updated User Codes to request new Registration Keys.
    The
    AADvance-Trusted SIS Workstation software
    is licensed for use with AADvance applications.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal