Assigning I/O Modules to the Trusted System
Trusted
SystemTo configure the SYSTEM.INI file, add I/O modules to the system layout of the
Trusted®
controller. At least one 8151 Communication Interface module
must also be added. If additional slots are required for the system, add an expander
chassis. When adding an expander chassis, a pair of 8311 Expander Interface modules must
also be included in the controller chassis. All Expander Chassis must be connected to the
Expander Interface modules.When adding modules, the layout that displays in the
System Configuration Tool
must
match the layout of the physical Trusted
controller and expander
chassis.It is recommended to disable slots with no configured modules and that will never be used
as companion slots or hot swaps. Disabling these slots removes them from the scanning
process and reduces the processing times. Disabling a slot disables all communications for
that slot; you can no longer hot swap a module or perform diagnostics on any module moved to
the disabled slot. For this reason, do not disable any companion slots or smart slots and
leave one slot active as a diagnostic slot.
Task | Procedure |
|---|---|
Add a module to a slot |
|
Empty a slot |
|
Add and connect an expander chassis |
|
Connect or disconnect an expander chassis |
|
Display the switch configuration for a connected expander chassis |
|
Disable an unused slot |
|
Provide Feedback