Modifying Cycle Timing

You can modify the cycle timing for controllers when you are running an application online.
Modify the cycle timing
ATTENTION:
Ensure that the
Cycle Timing
value combined with the
ISaGRAF Sleep Period
value is less than the
Maximum Scan Time
value. You can configure the
ISaGRAF Sleep Period
value and the
Maximum Scan Time
value in the System Configuration Tool. See System Configuration Tool.
  • From the
    Target Execution
    toolbar, enter the required
    Cycle Timing (ms)
    value. Setting the
    Cycle Timing
    to 0 allows the controller to execute cycles as fast as possible.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal