License Trusted applications
Use the
AADvance-Trusted SIS Workstation software
to create virtual machines that run on hardware
components, called targets.For
Trusted
applications, the AADvance-Trusted SIS Workstation software
is available for use with the following types of software licenses:- Demo License: delivered with the product and available for testing the product. This license provides a 60-day trial of the fully operational version of theAADvance-Trusted SIS Workstation softwareforTrustedapplications.
- Full License: obtained by manually activating an unlicensed version of the product. The Full License is a fully operational version of the product that enables the creation ofTrustedprojects that contain one device.
The obtained license is specific to a computer. The Full License persists through all
uninstall and reinstall operations. To move the license to another computer, contact the
support team to remove the license and then reauthorize it on another computer.
Provide Feedback