Trusted
Devices

A device corresponds to a
Trusted
controller.
Device names are limited to eight characters beginning with a letter or single underscore followed by letters, digits, and single underscores. Names cannot end with an underscore. Names cannot be reserved words, defined words, or data types.
Perform these tasks for devices:
  • Setting the properties of devices
  • Renaming devices
  • Building devices
  • Cleaning devices
  • Downloading devices
  • Simulating devices
  • Connecting devices
  • Updating devices
  • Displaying diagnostic information for devices
For devices, specify these properties:
Application Run-time Options
Description
Cycle Timing (ms)
ATTENTION:
Ensure that the
Cycle Timing
value combined with the
ISaGRAF Sleep Period
value is less than the
Maximum Scan Time
value.
You can configure the
ISaGRAF Sleep Period
value and the
Maximum Scan Time
value in the System Configuration Tool. See System Configuration Tool.
Amount of time, in milliseconds, allocated to each cycle. If a cycle is completed within the cycle timing period, the system waits until this period has elapsed before starting a new cycle. The cycle consists of scanning the physical inputs of the process to drive, executing the POUs of the device, then updating physical outputs. The
Trusted
controller executes the application code in real time. When the cycle time is set to 0, the controller starts the next cycle immediately after completing the last cycle.
The default cycle time is 0 ms.
Detect Errors
Store errors. Define the
Nb Stored Errors
option
.
Memory for Retain
Size of the memory space reserved for storing the values of retained variables. The values of these variables are stored in this memory at the end of each cycle for use if the target is restarted.
Nb Stored Errors
Number of entries, that is, the size of the queue (FIFO) in which detected errors are stored.
Compiler Options
Description
Generate Debug Information
Generate information required for debugging using step-by-step execution.
Miscellaneous
Description
Last Compilation Date
Date of the last compilation (build).
Last Compiled Version
Version number of the last compiled application image.
Serial Port Connection Information
Description
Baud Rate
Data transmission speed, defined in bits per second. Possible values are
600
,
1200
,
2400
,
4800
,
9600
, and
19200
; the default value is
19200
.
Data Bits
Number of data bits in a byte. Possible values are
7
or
8
.
Hardware Flow Control
AADvance-Trusted SIS Workstation software
controls the CTS and DSR lines to enable hardware handshaking during exchanges.
Parity
Parity type. Possible values are
None
,
Odd
,
Even
,
Mark
, or
Space
; the default value is
None
.
Stop Bits
Length of the stop bit. Possible values are
0
,
1
,
1.5
, or
2
.
Shared Connection Information
Description
Enable ISA68M
Enables the ISA68M target.
Enable Simulation
Enables simulating the application.
Network
Network used for communication. Possible values are
Serial
and
TCP/IP
. The default value is
TCP/IP
.
Retry
Number of tries for communication using a serial connection.
Serial Port or Port Category
Serial port used for communications. Possible values are
Simulator
,
Com1
,
Com2
,
Com3
,
Com4
,
Com5
,
Com6
,
Com7
,
Com8
,
Com9
,
Com10
,
Com11
,
User
, or
Ip
.
Timeout(s)
Communication timeout, expressed in seconds.
TCP/IP Connection Information
Description
Host Address
For TCP/IP connections, specifies the IP address of the host. The default port address is
127.0.0.1
Host Socket Port
Internet port number for a TCP/IP connection. For
Trusted
applications, the default port number is
6000
.
Task
Procedure
Set properties for a device
  • In the
    Application View
    , right-click the device, and then select
    Properties
    .
Rename a device
Renaming a device activates an automatic saving of the project.
  • In the
    Application View
    , right-click the device, then click
    Rename
    , and then type a name for the device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal