Loading
Press Release | November 29, 2012
Recent ActivityRecent Activity

Rockwell Automation Bundles Keys to Machine Control Design in One-Stop Solution

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail

Connected Components Accelerator Toolkit cuts design time and cost, optimizes control performance

MILWAUKEE, Nov. 29, 2012 — Rockwell Automation introduces the Connected Components Accelerator Toolkit (CCAT), a bundled, one-stop solution that simplifies and expedites complete, cost-effective, small-machine control design and implementation. The CCAT combines a simple, yet powerful controller with a full suite of compatible components and class-leading application development tools that enable OEMs to focus engineering and development resources on creating compelling and differentiating machine features.

The CCAT speeds the basic, common design functions that every machine design requires. By providing this functionality, the CCAT allows the OEMs to invest their design work in developing better, more competitive machines. The CCAT’s pre-configured Building Blocks include automation engineering design tools for comprehensive control application development from layout and component selection to troubleshooting. For example:

  • Quick Starts provide information to use the CCAT and set up individual components.
  • Selection tools and example bills of material streamline component and accessory selection.
  • Wiring diagrams and panel layout drawings, in native AutoCAD Electrical and EPLAN formats, save weeks of design effort.
  • Controller programming handles all communications, commands and status updates.
  • Common application starting system examples jump-start control design.
  • Sample human-machine interface (HMI) screens provide a superior operator interface, plus diagnostics, alarming and start-up assistance.

Connected Components Workbench software from Rockwell Automation supports the CCAT. Based on proven Rockwell Automation and Microsoft Visual Studio technology, the single, easy-to-acquire-and-install package simplifies controller programming, device configuration, and data sharing with the HMI editor for Allen-Bradley PanelView component products. The software makes it convenient and cost-effective for machine builders and end users to leverage a single platform that also supports other Allen-Bradley component-class devices, including drives, motion control and operator interface products.

About Rockwell Automation
Rockwell Automation, Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs over 22,000 people serving customers in more than 80 countries.

For more information:

  • Connected Components Accelerator Toolkit: http://www.rockwellautomation.com/components/connected/ccat.html
  • Connected Components Workbench software: http://ab.rockwellautomation.com/Programmable-Controllers/Connected-Components-Workbench-Software
  • Connected Components Accelerator Toolkit diagram: http://flic.kr/p/drtVpY

Media contacts:
Sarah Larson
Rockwell Automation
414.382.5910
selarson@ra.rockwell.com

Patty Hoffman
Padilla Speer Beardsley Inc.
612.455.1781
phoffman@padillaspeer.com

Allen-Bradley, Connected Components Workbench, LISTEN. THINK. SOLVE. and PanelView are trademarks of Rockwell Automation, Inc.
Trademarks not belonging to Rockwell Automation are property of their respective companies.

Published November 28, 2012


  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Press Releases
  5. Chevron LeftChevron Left Rockwell Automation Bundles Keys to Machine Control Design in One-Stop Solution