Access Controller Front Port Diagnostics
You can use an MSG instruction to access minor faults and
EtherNet/IP™
port diagnostics that are related to Front Port Crossload mode on the controller.Useful diagnostics include the following:
- Status of either port
- Number of packets lost during the last 24 hours for either port
- Total time in seconds that a warning has been active on either port
For more information about Front Port Crossload mode, see Configure Front Port Crossload mode.
Provide Feedback