Connect a Contactor to the Bus

  1. Place the communication interface module at the front of the 100-E contactor cover.
  2. Align the link bars into the slots of the 100-E contactor, then push the communication interface module toward the 100-E contactor.
    Align the Link Bars into the Slots of the Contactor
    Align link bars to slots of contactor
  3. Slide the communication interface module in parallel direction to the 100-E contactor front cover until the plunger comes into contact with the crossbar on the 100-E contactor.
    Make Contact with the Crossbar on the Contactor
    Properly seated module
Reseat the Communication Interface Module on a Contactor
If the communication interface module must be reseated:
  • Pull the plastic detent clip away from the front of the 100-E contactor and slide the communication interface module upward and away from the 100-E contactor.
  • Repeat steps 1...3.
Reseat the Module on the Contactor
Reseat the module
Adjust the Communication Interface Module: 104-E Reversing Contactors
The 104-E-INT-D and 104-E-INT-X modules can be adjusted to various sizes to accommodate the 100-E contactor.
To adjust, slightly flex apart the sides of the double-wide cover during adjustment.
Approximate dimensions are shown in millimeters (inches). Dimensions are not intended to be used for manufacturing purposes.
Adjust the Reversing Contactors
Item
Description
Size 1 and 2
Size 3
Size 3.5
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal