Refresh a model
To import changes you make in
Studio 5000 Logix Designer
into Studio 5000 Smart Object Configurator
, refresh the information model. Refreshing the model ensures that model information match in both Studio 5000 Logix Designer
and Studio 5000 Smart Object Configurator
.
TIP:
- If the safety controller lock is enabled, the SOC fails to update the controller. The workaround is to unlock it to refresh the model.
- If the safety controller is signed, remove the signature before editing Smart Objects (resigning a controller can invalidate any safety network associated with that signature).
To refresh a model
- Make changes inStudio 5000 Logix Designer.
- InStudio 5000 Smart Object Configurator, selectRefresh information model.
Provide Feedback