Modify the OPC code quality value

A
FactoryTalk Smart Object
transmits quality code values to
FactoryTalk Edge Gateway
based on OPC quality. By default, the OPC quality code value in a
Studio 5000 Smart Object Configurator
is 192.
Create logic in the
Logix 5000
application to change the OPC quality values that
FactoryTalk Smart Object
instances transmit to
FactoryTalk Edge Gateway
.
To modify the OPC quality code value of a
FactoryTalk Smart Object
  1. In the
    Logix 5000
    application, create logic as needed.
  2. Move the new OPC value to the backing tag of the
    FactoryTalk Smart Object
    (Smart Object.Inp_Quality).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal