Install base code

Open the desired Logix application in
Studio 5000 Logix Designer
and then launch
Studio 5000 Smart Object Configurator
.
Connect to a
Studio 5000 Logix Designer
.acd project file to run
Studio 5000 Smart Object Configurator
. To create a
FactoryTalk Smart Object
, the .acd project file requires
FactoryTalk Smart Object
base code: program, routine, and rung.
If
FactoryTalk Smart Object
base code is not in the project, install the
FactoryTalk Smart Object
base code.
To install base code
  1. Double-click an .acd project file.
  2. In
    Studio 5000 Logix Designer
    , select
    Tools >
    Studio 5000 Smart Object Configurator
    .
    If the project includes
    FactoryTalk Smart Object
    base code,
    Studio 5000 Smart Object Configurator
    launches with the
    FactoryTalk Smart Object
    information model.
  3. If
    FactoryTalk Smart Object
    base code is not in the project, install the
    FactoryTalk Smart Object
    base code.
    1. In
      Insert base components
      select a program. The program can be in the fastest executing task within the project.
    2. Select a routine. The routine must be ladder logic.
    3. Select a rung number.
  4. Select
    Add
    .
    Code is injected into the controller. The
    Assets
    tab in the
    Controller Organizer
    updates. A
    FactoryTalk Smart Object
    timer appears in the ladder logic according to the location set for the
    FactoryTalk Smart Object
    base code. A first element called
    Information model
    appears in
    Studio 5000 Smart Object Configurator
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal