Generate a CSV template to create
FactoryTalk Smart Object
instances

Generate a CSV template that contains the columns required for creating
FactoryTalk Smart Object
instances.
After using the CSV template to create
FactoryTalk Smart Object
instances quickly, import the new
FactoryTalk Smart Object
instances into
Studio 5000 Smart Object Configurator
.
TIP:
The generated CSV template differs from the CSV file that is created when exporting full configuration values. The generated CSV template does not contain read-only headings.
To generate a CSV template to create
FactoryTalk Smart Object
instances
  1. Select
    Export
    .
  2. In
    Export
    , select
    Creation template
    .
  3. Select
    Export
    .
  4. Select a folder and then type a name for the CSV file.
  5. Select
    Save
    .
    An empty template appears in your folder.
    NOTE:
    The CSV file exported from the Smart Object Configurator application may contains sensitive and critical information. Ensure that the data is always secured or encrypted and proper permissions are set to that file.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal