Export FactoryTalk Smart Object configuration values
FactoryTalk Smart Object
configuration valuesExport
FactoryTalk Smart Object
configuration values to a CSV file to update values quickly. Use the CSV file to filter and modify FactoryTalk Smart Object
configuration values. After modifying the
FactoryTalk Smart Object
configuration values in the CSV file, import the FactoryTalk Smart Object
configuration values to Studio 5000 Smart Object Configurator
.To export
FactoryTalk Smart Object
configuration values- SelectExport
.
- SelectFull configuration.
- SelectExport.
- Select a location and type a file name.
- SelectSave.A CSV file is created.
- Modify the spreadsheet. Columns that are read-only contain (r) in the column heading.NOTE:The CSV file exported from the Smart Object Configurator application may contains sensitive and critical information. Ensure that the data is always secured or encrypted and proper permissions are set to that file.
Provide Feedback