Configure Add-On Instructions
Configure Add-On Instructions (AOIs) to add them to your
FactoryTalk Smart Object
model.The hierarchy of an Add-On Instruction model does not follow the same hierarchy as an information model. In Add-On Instruction models, nodes and data types can appear at the top of the model hierarchy.
TIP:
The Add-On Instruction must use ladder logic.
To configure Add-On Instructions
- InStudio 5000 Logix Designer, create an Add-On Instruction.
- InStudio 5000 Smart Object Configurator, selectConfigure AOIs.
- SelectRefresh information modelto see the new Add-On Instruction.
- Select the new Add-On Instruction.
- SelectAdd
and then select a data type.
- Configure the data type properties.
- SelectAdd. A new model appears with the new data type.TIP:To add data type to an existing information model, right-clickModel, and then select a data type.
Provide Feedback