Bulk import new FactoryTalk Smart Object instances from a CSV file
FactoryTalk Smart Object
instances from a CSV fileAfter updating a CSV file with new
FactoryTalk Smart Object
instances, bulk import the new FactoryTalk Smart Object
instances into Studio 5000 Smart Object Configurator
. To bulk import new
FactoryTalk Smart Object
instances from a CSV file- SelectImport
.
- SelectNewFactoryTalk Smart Objectinstances.
- SelectImport.
- Select the CSV file to import.TIP:The CSV file that is based on the creation template contains different headings from the CSV created when exporting a full configuration. Import the correct CSV file.
- SelectOpen.The information model contains the new values.TIP:If you have a long list of errors, inImport results, copy the errors to the clipboard and then copy the errors to a preferred text editor for review.
Provide Feedback