Add a REAL data type to an information model

Add a REAL data type to a
FactoryTalk Smart Object
information model. Set the basic collection properties to describe how the REAL
FactoryTalk Smart Object
collects data.
To add a REAL data type to an information model
  1. Perform one of these actions:
    • Right-click a node and then select
      New REAL
      .
    • Select a node, select
      Add
      , and then select
      REAL
      .
      The
      Add REAL
      FactoryTalk Smart Object
      instances
      dialog box appears.
  2. Set these basic properties:
    • Name
      : Name of the data displayed in the information model. See Rules for names and backing tags.
    • Backing tag
      : Name of the backing tag in the controller. A backing tag is created in the
      Studio 5000 Logix Designer
      project that contains the configuration information for the
      FactoryTalk Smart Object
      .
    • Source value tag (optional)
      : Location where the data gathers.
    • Program
      : Controller program where the node resides.
    • Routine
      : Controller routine where the node resides.
    • Insert at
      : Location to add a rung in the routine where the
      FactoryTalk Smart Object
      appears.
    • Insert at end
      : Location at the end of a routine where the
      FactoryTalk Smart Object
      appears.
  3. Set these data collection parameters:
    • On parent or periodic
      : When this checkbox,
      On programmatic
      , and
      On value
      checkboxes are clear, data collection for this data value does not occur.
      TIP:
      It is possible to have multiple triggers active at once.
      • Parent
        : When Parent is triggered, the
        FactoryTalk Smart Object
        is also triggered.
      • Periodic
        : Interval in seconds when data is sampled in the source tag.
    • On programmatic
      : Ladder logic that triggers the condition for collection.
    • On value, when the value changes by
      : Data is sampled each time that it changes based on the value in engineering units (positive number).
  4. Select
    Add
    .
    A new rung appears in the ladder logic. The real
    FactoryTalk Smart Object
    appears in the
    FactoryTalk Smart Object
    tree.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal