No support of embedded Ethernet port with redundancy

For the ControlLogix 5580 and GuardLogix 5580 controllers, redundancy does not support any use of the controller's Ethernet front port, including I/O, messaging, and downloading.
Select
Yes
to enable redundancy and remove support of the embedded Ethernet port. Select
No
to maintain support of the embedded Ethernet port and remove redundancy.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal