DANGER Changing Electronic Keying

IMPORTANT: Changing Electronic Keying parameters online interrupts connections to the device and any devices that are connected through the device. Connections from other controllers can also be broken.
A loss of data may occur if an I/O connection to a device is interrupted.
For more information on Electronic Keying, see Electronic Keying in Logix 5000 Control Systems Application Technique, publication LOGIX-AT001.
To do this:
Select:
Change the electronic keying option.
OK
Cancel the operation.
Cancel
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal