Parameter List page
Use the
Parameter List
tab to:- Display and configure additional attributes for the axis
- View a subset of the attributes based on the parameter group
The list of items varies accordingly to the type of Axis Configuration or filtering that you select in the
Parameter Group
list. The displayed list can be:- All of the parameters (the default if the page is accessed directly)
- A subset, if the group pull-down was used to select a specific subset
- The parameters from which you accessed this page if you clicked theParametersbutton on the page. For example, if you clicked theParametersbutton on theScalingpage, theParameter Groupis set toScaling.TIP:
- The parameters in the grid behave the same way (with regard to their appearance and operation) as the parameters do on their associated page. For example, if you change an attribute on a page from enabled to read-only or to disappear altogether, then that attribute is changed in the same way in this grid.
- TheParameter Listpage may contain more attributes than the associated page. In some cases, attributes that are contained on theParameter Listpage are not contained on the associated page.
TIP:
To open the Parameter List page:
- In theController Organizer, expand theMotion Groupsfolder, and double-click an axis.
- From theAxis Propertiesdialog box, inCategories, clickParameter List.
The Parameter List includes these parameters.
Parameter | Description |
Parameter Group | Select a parameter from the list and view the attributes on the grid. Settings on the General page, such as the Axis Configuration , Feedback Configuration , and Associated Module determine which attributes display for the selected parameter.The available parameter groups are:
TIP:
The
General , Status , and
Fault Log dialog boxes are not part of the parameter list. The
Parameter Group lists only dialog boxes that contain valid attributes for
the current configuration. If a dialog box is blank because all attributes on the
dialog box are optional and not supported by the current drive, that dialog box
does not appear in Parameter list. |
Grid | Displays the set of attributes that are valid for the current configuration of the axis. Also displays attributes from the selected Parameter Group .The grid columns are:
Double-click the Name heading to sort the grid rows. The columns can be re-sized but revert back to the default size when the dialog box closes. |
Associated Page | Returns to the associated dialog box. For example, when accessing this dialog box from the Frequency Control dialog box, click Associated Page to return to the Frequency Control dialog box. |
Provide Feedback